Memory Cards for Industrial Ethernet switches
Description
- Redundant storage of switch configuration
- Prioritized loading the cash card at Power-UP
- Each Memory Card has unique MAC address
- Wide temperature range
- Industrial grade SD Memory Card
Description
- Redundant storage of switch configuration
- Prioritized loading the cash card at Power-UP
- Each Memory Card has unique MAC address
- Wide temperature range
- Industrial grade SD Memory Card
Standards
International : Manufacturer specificationNational : Customer specification
Description
Nexans memory cards are redundant encrypted storage (AES256) for Nexans Industrial and compact ruggedized Ethernet switches which always stores its complete and most actual configuration and firmware automatically. There are different formats: SD and micro SD for industrial and ruggedized compact IND switches respectively.
To make network maintenance processes easier, Nexans memory cards have unique MAC address fixed on it. Switch replaces its own MAC address with the one read from memory card. In case of a switch replacement the SD card needs to be removed from one switch and installed into the new one. The MAC-address, configuration and firmware will be taken on by the new switch from this SD-card. So no changes in the network policy or pre-setup works need to be made as the system will see the same switch as before.
The special version of Memory Card is equipped with MRP Multi license is available for iGigaSwitch family. Memory Card with MRP license activate the usage of Media Redundancy Protocol in according to IEC 62439.
- Encrypted data storage (AES256) provides the highest level of protection for the saved configuration, firmware, etc.
- Operating temperature range of the memory cards: -40…+85oC