Medium-voltage jumpers

  • Medium-voltage jumpersCustomized jumpers are lengths of MV cable from 1 meter to tower height, equipped on both sides with accessories to connect generators, transformers and switchgears.

All jumpers are pretested in the factory to assure immediate and fault-free installation.

These cables are part of our Windlink® solutions designed by Nexans to respond the very demanding expectations of the wind turbine market.


Related products and solutions


WINDLINK® Low Voltage cables up to 1,8/3kV
Special Cables/Wind turbines dedicated cables

Cables in the Wind Industry, especially for wind turbines and for loop installation on the top of the tower are facing severe torsion constraints due to the rotation of the nacelle.
Due to the minimum 20 years life time of wind turbines, Nexans brings an appropriate answer to all O.E.M requirements and specifications.
Torsion tests simulate a 20-year life time in a turbine. To meet this requirement, cables have to comply with a complete test which depends on customers’ specification.
Nexans has developed low voltage loop cables (up to 1kV) that reliably transmit energy produced in the generator to the transformer, usually located at the base of the tower. They come in Low-Smoke Zero-Halogen (LSZH) versions, and are also oil, abrasion, UV and ozone-resistant.