Low-voltage kits

  • Low-voltage sets and kitsTo facilitate assembly, Nexans provides pre-connectorized kits which bundle energy, control and data cables for wind turbine electronics.
  • Cut-to-length, pre-connectorized, all-power cables are supplied to tower manufacturers for generator-to-switchgear-to-main-powerline links.

Nordex appreciates the consolidation of several cable types into a single purchase.

These cables are part of our Windlink® solutions designed by Nexans to respond the very demanding expectations of the wind turbine market.


Related products and solutions


WINDLINK® Low Voltage cables up to 1,8/3kV
Special Cables/Wind turbines dedicated cables

Cables in the Wind Industry, especially for wind turbines and for loop installation on the top of the tower are facing severe torsion constraints due to the rotation of the nacelle.
Due to the minimum 20 years life time of wind turbines, Nexans brings an appropriate answer to all O.E.M requirements and specifications.
Torsion tests simulate a 20-year life time in a turbine. To meet this requirement, cables have to comply with a complete test which depends on customers’ specification.
Nexans has developed low voltage loop cables (up to 1kV) that reliably transmit energy produced in the generator to the transformer, usually located at the base of the tower. They come in Low-Smoke Zero-Halogen (LSZH) versions, and are also oil, abrasion, UV and ozone-resistant.